SLUSFR2 November 2024 BQ21088
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Depending on the configuration set on pushbutton long press action register bits, the device will perform a ship mode entry, shutdown mode entry, or hardware reset or completely ignore the long button press action.Toggling the /CE pin will restart the timer for the long press button when VIN is present.
To wake up the device from ship mode , there are two methods: a valid VIN power up or holding the TS/MR button for a time tSHIPWAKE.