SLUSD08A May 2017 – January 2018
PRODUCTION DATA.
The voltage at TS is monitored to determine that the battery is at a safe temperature during charging. This device uses JEITA temperature profile which has four temperature thresholds. Refer to Specifications for the detailed thresholds number.
The TS circuit is shown in Figure 18. The resistor values can be calculated using Equation 1 and Equation 2.