SLUSBZ9C August 2015 – September 2016 BQ25120 , BQ25121
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI's customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
A typical design is shown in Figure 35. This design uses the BQ25120 with external resistors for ILIM, IPRETERM, and ISET. These are not needed if these values are set with a host controller through I2C commands. This design also shows the TS resistors, which is also optional.
When powering up in default mode the battery voltage is the default for the part (4.2 V), the SYS output is the default (1.8 V). External resistors set the charge current to 40 mA, the termination current to 10% (4 mA), and the input current limit to 100 mA. If the I2C interface is used the part goes to the internal default settings until changed by the host.
This application is for a low power system that has varying loads from less than 10 mA up to 300 mA. It must work with a valid adaptor or USB power input. Below are some of the key components that are needed in normal operation. For this example, the fast charge current is 50 mA, input current limit is 400 mA and the pre-charge and termination current is 10% of the fast charge current.
See Figure 35 for an example of the application diagram.
Refer to the Buck (PWM) Output section for the detailed procedure to determine the optimal inductance and capacitance for the buck output.
KISET = 200 AΩ from the Specifications table
Select the closest standard value, which in this case is 4.99 kΩ. Connect this resistor between ISET pin and GND.
KILIM = 200 AΩ from the Specifications table
Select the closest standard value, which in this case is 499 Ω. Connect this resistor between ILIM pin and GND.
According to Table 3, the RIPRETERM is 4990 Ω for 10% termination threshold. Therefore, connect a 4.99 kΩ resistor between IPRETERM pin and GND.
The voltage at TS is monitored to determine that the battery is at a safe temperature during charging. This device uses JEITA temperature profile which has four temperature thresholds. Refer to Specifications for the detailed thresholds number.
The TS circuit is shown in Figure 16. The resistor values can be calculated using Equation 1 and Equation 2.
TA = 25°C | VSYS = 1.2 V |
TA = 25°C | VSYS = 1.8 V |
TA = 25°C | VSYS = 3.3 V |
TA = 25°C | VSYS = 1.5 V |
TA = 25°C | VSYS = 2.5 V |
TA = 25°C | VSYS = 1.2 V |
TA = 25°C | VSYS = 1.8 V |
TA = 25°C | VSYS = 3.3 V |
ILOAD = 10 µA |
ILOAD = 1 mA |
ILOAD = 100 mA |
ILOAD = 300 mA |
VSYS = 1.8 V |
VSYS = 2.5 V |
VSYS = 1.2 V |
VSYS = 2.1 V |
VSYS = 3.3 V |
TA = 25°C | VSYS = 1.5 V |
TA = 25°C | VSYS = 2.5 V |
TA = 25°C | VSYS = 1.2 V |
TA = 25°C | VSYS = 1.8 V |
TA = 25°C | VSYS = 3.3 V |
TA = 25°C | VSYS = 1.5 V |
TA = 25°C | VSYS = 2.1 V |
ILOAD = 100 mA |
ILOAD = 10 mA |
ILOAD = 200 mA |
VSYS = 1.2 V |
VSYS = 2.1 V |
VSYS = 3.3 V |
VSYS = 1.8 V |
VSYS = 2.5 V |
VSLSDO = 0.8 V |
VSLSDO = 1.8 V |
VSLSDO = 3.3 V |
VSLSDO = 1.2 V |
VSLSDO = 2.5 V |
VSLSDO = 1.2 V |
VSLSDO = 2.5 V |
VSLSDO = 0.8 V |
VSLSDO = 1.8 V |
VSLSDO = 3.3 V |
Wake1 = 500 ms | Wake2 = 1 s |
RESET = 4 s |
RESET = 14 s |
Wake1 = 50 ms | Wake2 = 1.5 s |
RESET = 8 s |