SLUSF40 October 2024 BQ25190
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Ship mode is the lowest quiescent current state for the device with BATFET being turned off.
Ship mode can be initiated by writing b10 to the EN_RST_SHIP register bits. If the ship mode setting is set, the device will wait until the input source is removed to enter ship mode. When an I2C command is given to set the device to enter ship mode, the device waits for 1 second before the implementation.
Ship mode can also be initiated with MR pulled low for tLPRESS when PB_LPRESS_ACTION is writen to b10. Figure 7-6 shows this behavior. The power-down sequence starts when MR pin is pulled low for tLPRESS. The ship mode is entered after SYS pulldown with power-down sequence completion and MR pin is above the low threshold.
The device can exit ship mode by adapter insertion (VIN > VIN_UVLOZ) or MR pin is pulled low for tSHIPWAKE with VBAT>VBUVLO.For the device to reliably exit ship mode by adapter insertion, VIN needs to be higher than VIN_UVLOZ for at least 30ms.