SLUSF40A October 2024 – December 2024 BQ25190
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The integrated power rails can be configured to be power up or power down in a programmable sequence. In addition, the GPIO pins can be configured to be push-pull power sequencer output which can enable or disable external power rails in the sequence. If at least one of the integrated power rail is configured to be in the sequence or at least one of the GPIO pins is configured to be sequencer output, it means that the power sequence is used. Otherwise, it means that the power sequence is not used. An integrated power rail is a sequence power rail if it is configured to be in the sequence. For Buck or Buck-boost, it can be individually enabled or disabled by I2C or GPIO if it's not a sequence power rail. Therefore, Buck or Buck-boost can be in sequence mode or individual mode. For LDO1 or LDO2, it can be individually enabled or disabled by I22 or GPIO, or always on if it is not a sequence power rail. Therefore, the LDO1 and LDO2 can be in sequence mode, individual mode, or always-on mode.