SLUSF40 October 2024 BQ25190
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
To prevent deep discharge of the battery, the device integrates a battery depletion protection feature which disengages the BAT to SYS path when voltage at the battery drops below VBATDEPL programmed by BATDEPL bits in the CHARGECTRL1 register.
In battery only mode, the BATFET is turned on if VBAT rises to be higher than VBATDEPLZ. The BATFET is turned off if VBAT falls to be lower than VBATDEPL.
BATDEPL status is reported by BATDEPL_FAULT_STAT bit. BATDEPL_FAULT_FLAG is set to 1 if battery depletion is detected. a 128-μs pulse (INT pin pulled down) is sent on INT to notify the host if not masked by BATDEPL_FAULT_MASK.