SLUSF40 October 2024 BQ25190
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The device integrates two ultra-low quiescent current LDOs, LDO1 and LDO2, which can also be configured to bypass mode to operate as a switch. Therefore, they can provide either a regulated output or gate power to external loads. LDO1 and LDO2 have dedicated input pins VINLS1 and VINLS2 and can support up to 200 mA load current.
The output of voltage of LDO1/LDO2 is programmable using LDO1_VOUT_SET/LDO2_VOUT_SET bits from 0.8V to 3.6V in 50mV steps. The LDO1/LDO2 does not actively discharge the output capacitor if the actual VOUT is higher than the target. The LDO1/LDO2 turns off the internal FET until the actual VOUT reaches the target. Therefore, the actual VOUT slew rate is dependent on the load at the output in this case.
Setting the LDO1_LDO_SWITCH_CONFG/LDO2_LDO_SWITCH_CONFG will configure LDO1/LDO2 to operate in either LDO mode or bypass (switch) mode. Note that in order to change the configuration, LDO1/LDO2 must be disabled first, then the LDO1_LDO_SWITCH_CONFG/LDO2_LDO_SWITCH_CONFG takes effect.
Whether always-on LDO1 is operating in LDO1-ON Ship mode is dependent on the LDO1_SHIP_AO bit setting.If LDO1_SHIP_AO is 1 when power-down sequence is started to enter the Ship mode, the LDO1 VOUT is set by LDO1_VOUT_SET if LDO1 was in LDO mode and LDO1's ON/OFF status is latched if LDO1 was in bypass mode. For LDO1_SHIP_AO to be effective, LDO1_EN_SET needs to be set to b111.
LDO1/LDO2 has the output discharge function. The purpose of this function is to ensure a defined down-ramp of the output voltage when LDO1/LDO2 is disabled and to keep the output voltage close to 0V. The discharge function is only active when LDO1/LDO2 is disabled. Do not rely on the active discharge circuit for discharging a large amount of output capacitance after the input supply has collapsed because reverse current can possibly flow from the output to the input. This reverse current flow can cause damage to the device. Limit reverse current to no more than 5% of the device rated current for a short period of time.
When LDO1/LDO2 does not have valid input power at VINLS1/VINLS2, it should be disabled.