SLUSF40 October 2024 BQ25190
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The device has an internal pulldown on the SYS pin which is enabled in the following cases:
STATE | NOTES |
---|---|
ship mode | Pulldown on SYS is enabled with power-down sequence. Then the device enters the ship mode. |
HW_RESET | Pulldown on SYS is enabled with power-down sequence. The SYS pull-down is retained until the autowake timer expires. |
SYS_MODE = b11 (SYS pulldown mode) | Pulldown on SYS is enabled with power-down sequence. The SYS pull-down is retained until SYS_MODE is changed to b00/b01/b10 or VIN is toggled. |