SLUSD83C june 2018 – may 2023 BQ25713 , BQ25713B
PRODUCTION DATA
REG0x22[7:0] and REG0x23[0] reports which event in the profile triggers PROCHOT if the corresponding bit is set to 1. The status bit can be reset back to 0 after it is read by host, when the current PROCHOT event is not active any more.
Assume there are two PROCHOT events, event A and event B. Event A triggers PROCHOT first, but event B is also active. Both status bits will be HIGH. At the end of the 10 ms PROCHOT pulse, if any of the PROCHOT event is still active (either A or B), the PROCHOT pulse is extended.