SLUSFK8 April 2024 BQ25770G
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
REG0x21[8:0] reports which event in the profile triggers PROCHOT if the corresponding bit is set to 1. The status bit can be reset back to 0 after it is read by the host, when the current PROCHOT event is not active any more.
Assume there are two PROCHOT events, event A and event B. Event A triggers PROCHOT first, but event B is also active. Both status bits will be HIGH. At the end of the 10 ms PROCHOT pulse, if any of the PROCHOT event is still active (either A or B), the PROCHOT pulse is extended.