SLUS696C June 2006 – February 2019
PRODUCTION DATA.
Unlike the general use pages, the status bytes read 0xFF when not programmed and a bit is programmed from 1 to 0. A zero represents the active state.
Address 0x0007 Reserved
Default value is 0xFF
Address 0x0006 Key Index
The host can determine which one of multiple keys was programmed into the bq26100 device by reading the key index value.
Address 0x0005 – 0x0001 Page Redirection
A pointer for alternative page information, these bytes can be used if information in the original page has been invalidated. The host can read these locations and direct reads and/or writes to the page pointed to by the value in the register. For example, if the data in page 2 is corrupted by an incorrectly written data value, and the corrected data is in page 1, the value written to address 0x0003 would be 0xFE (1’s complement value of 0x01). Upon reading address 0x0003, the host would receive 0xFE and would take the 1’s complement to determine that page 1 contains redirected data.
ADDRESS | PAGE REDIRECTED |
---|---|
0x0005 | Page 4 |
0x0004 | Page 3 |
0x0003 | Page 2 |
0x0002 | Page 1 |
0x0001 | Page 0 |
There is no hardware mapping of the page redirection bytes. The host is responsible for sending the correct address for a redirected page.