A capacitor, of value at least 0.47 µF, is connected between the VDD pin and VSS. The capacitor should be placed close to the gauge IC and have short traces to both the VDD pin and VSS.
It is required to have a capacitor, at least 1.0 µF, connect between the BAT pin and VSS if the connection between the battery pack and the gauge BAT pin has the potential to pick up noise. The capacitor should be placed close to the gauge IC and have short traces to both the VDD pin and VSS.
If the external pullup resistors on the SCL and SDA lines will be disconnected from the host during low-power operation, it is recommended to use external 1-MΩ pulldown resistors to VSS to avoid floating inputs to the I2C engine.
The value of the SCL and SDA pullup resistors should take into consideration the pullup voltage and the bus capacitance. Some recommended values, assuming a bus capacitance of 10 pF, can be seen in Table 4.
Table 4. Recommended Values for SCL and SDA Pullup Resistors
VPU
1.8 V
3.3 V
RPU
Range
Typical
Range
Typical
400 Ω ≤ RPU ≤ 37.6 kΩ
10 kΩ
900 Ω ≤ RPU ≤ 29.2 kΩ
5.1 kΩ
If the GPOUT pin is not used by the host, the pin should still be pulled up to VDD with a 4.7-kΩ or 10-kΩ resistor. After the OTP has been programmed, it is recommended that PROG be connected to the SDA line with a 470-KΩ resistor so that in cases where the device is in SHUTDOWN, toggling PROG can wake the gauge up from the SHUTDOWN state.
If the battery pack thermistor is not connected to the BIN pin, the BIN pin should be pulled down to VSS with a 10-kΩ resistor.
The BIN pin should not be shorted directly to VDD or VSS.
The actual device ground is the center pin (B2). The C1 pin is floating internally and can be used as a bridge to connect the board ground plane to the device ground (B2).