SLUSCM6E June 2016 – April 2019 BQ35100
PRODUCTION DATA.
The ACCUMULATOR mode (ACC) is chemistry-independent and accumulates the passed discharge of the battery when the gauge is enabled, but also provides no gas gauging data, such as remaining state-of-health (RSOC), full charge capacity (FCC), or end-of-service (EOS) indication. This is the default configuration as it is also the required mode for the device when it is calibrated. Once calibration is completed, the device can be set to the appropriate gauging mode or left in the default mode.
To configure the BQ35100 fuel gauge to use the ACCUMULATOR mode, the following data flash configuration variables must be configured correctly. For more details, including information on Operation Config A [GMSEL], see the BQ35100 Technical Reference Manual (SLUUBH1).
To use ACCUMULATOR mode, follow these steps: