SLUSCM6E June 2016 – April 2019 BQ35100
PRODUCTION DATA.
STATE-OF-HEALTH mode is typically used with lithium manganese dioxide (Li-MnO2) cells as the voltage vs. state-of-health (SOH) profile has a defined slope to enable accuracy.
To configure the BQ35100 gauge to use the STATE-OF-HEALTH mode, the following data flash configuration variables must be configured correctly. For more details, including information on Operation Config A [GMSEL], see the BQ35100 Technical Reference Manual (SLUUBH1).
To use STATE-OF-HEALTH mode, follow these steps: