The BQ76907 device supports a random
connection sequence of cells to the device during pack manufacturing. For example, cell-6 in
a 7-cell stack might be first connected at the input terminals leading to pins VC6 and VC5,
then cell-2 may next be connected at the input terminals leading to pins VC2 and VC1, and so
on. It is not necessary to connect the negative terminal of cell-1 first at VC0. As another
example, consider a cell stack that is already assembled and cells already interconnected to
each other, then the stack is connected to the PCB through a connector, which is plugged or
soldered to the PCB. In this case, the sequence order in which the connections are made to
the PCB can be random in time, they do not need to be controlled in a certain sequence.
There are some restrictions to how the cells
are connected during manufacturing:
- To avoid misunderstanding, note that
the cells in a stack cannot be randomly connected to any VC pin on the device, such as
the lowest cell (cell-1) connected to VC7, while the top cell (cell-7) is connected to
VC1, and so on. It is important that the cells in the stack be connected in ascending
pin order, with the lowest cell (cell-1) connected between VC1 and VC0, the next higher
voltage cell (cell-2) connected between VC2 and VC1, and so on.
- The random cell connection support is
possible due to high-voltage tolerance on pins VC1–VC7.
Note: VC0 has a lower voltage tolerance. This
is because VC0 should be connected through the series-cell input resistor to the VSS
pin on the PCB, before any cells are attached to the PCB. Thus, the VC0 pin voltage is
expected to remain close to the VSS pin voltage during cell attach. If VC0 is not
connected through the series resistor to VSS on the PCB, then cells cannot be
connected in random sequence.
- Each of the VC1–VC7 pins includes a
diode between the pin and the adjacent lower cell input pin (that is, between VC7 and
VC6, between VC6 and VC5, and so on), which is reverse biased in normal operation. This
means an upper cell input pin should not be driven to a low voltage while a lower cell
input pin is driven to a higher voltage, since this would forward bias these diodes.
During cell attach, the cell input terminals should generally be floating before they
are connected to the appropriate cell. It is expected that transient current will flow
briefly when each cell is attached, but the cell voltages will quickly stabilize to a
state without DC current flowing through the diodes. However, if a large capacitance is
included between a cell input pin and another terminal (such as VSS or another cell
input pin), the transient current may become excessive and lead to device heating.
Therefore, it is recommended to limit capacitances applied at each cell input pin to the
values recommended in the specifications.