SLUSF60 December 2023 BQ77307
PRODUCTION DATA
The BQ77307 device includes two security modes: SEALED and FULLACCESS, which can be used to limit the ability to view or change settings.
Selected settings in the device can be modified while the device is in operation through supported commands and subcommands, but in order to modify all settings, the device must enter CONFIG_UPDATE mode (see CONFIG_UPDATE Mode), which stops device operation while the settings are updated. After the update is completed, the operation is restarted using the new settings. CONFIG_UPDATE mode is only available in FULLACCESS mode.
The BQ77307 device implements a key-access scheme to transition between SEALED and FULLACCESS modes. Changing from SEALED to FULLACCESS requires that a unique set of keys be sent to the device through subcommands. Refer to BQ77307 Technical Reference Manual for more details.