SLUSCD0B August 2015 – November 2018
PRODUCTION DATA.
The bq78350-R1 device is powered directly from the 2.5-V REGOUT pin of the bq769x0 companion AFE. An input capacitor of 0.1 µF is required between VCC and VSS and should be placed as close to the bq78350-R1 device as possible.
To ensure a fast ramp-down voltage on the VCC pin during a MAC Shutdown() command, connect a 1-k pullup resistor between the PWRM pin and VCC, and connect a 1-µF capacitor between PWRM and VSS.
To ensure correct power up of the bq78350-R1 device, a 100-k resistor between MRST and VCC is also required. See the Schematic for further details.