SLUSEC2A December 2021 – November 2023 BQ79631-Q1
PRODUCTION DATA
The CONTROL1[ADDR_WR] bit enables the auto-addressing mode. In this mode, the device turns off its COMH/COML (depends on the [DIR_SEL] setting) transmitter for one communication frame (following the auto-addressing procedure, that will be its own device’s address), clear the CONTROL1[ADDR_WR] = 0. When the next communication is received (following the auto-addressing procedure, it will be the next device’s address), the device will forward the communication to the next device.