SLUSE48B May 2021 – November 2023 BQ79652-Q1 , BQ79654-Q1 , BQ79656-Q1
PRODUCTION DATA
Cell balancing can be paused by one of three methods:
The first two conditions are described in Section 9.3.3.1.3. The third pause condition is a MCU-controlled pause action usually used during a diagnostic check that involves the CB path. MCU can pause cell balancing through the [CB_PAUSE] bit at any given time once balancing starts.
When the cell balancing is paused due to any of the pause methods, the pause activity is the same:
Once the device exits the cell balancing pause state, the cell balancing resumes. Cell balancing timers will continue the count down. CB channels with non-zero values in their timers will continue with the balancing.