SWRS226B February 2020 – May 2021 CC3230S , CC3230SF
PRODUCTION DATA
The CC3230x device can accept an external TCXO/XO for the 40-MHz clock. In this mode of operation, the clock is connected to WLAN_XTAL_P (pin 23). WLAN_XTAL_N (pin 22) is connected to GND. The external TCXO/XO can be enabled by TCXO_EN (pin 21) from the device to optimize the power consumption of the system.
If the TCXO does not have an enable input, an external LDO with an enable function can be used. Using the LDO improves noise on the TCXO power supply.
Figure 8-12 shows the connection.
Section 8.16.5.4.1 lists the external Fref clock requirements.