To receive notification of
documentation updates — including silicon errata — go to the CC3235MOD product
folder on ti.com. In the upper-right corner, click on Alert me to
receive a weekly digest of any product information that has changed. For change
details, check the revision history of any revised document.
The current documentation that
describes the processor, related peripherals, and other technical collateral is as
follows.
Application Reports
SimpleLink™ CC3135, CC3235 Wi-Fi® Internet-on-a chip™
Networking Sub-System Power Management
This application report describes the best practices for
power management and extended battery life for embedded low-power Wi-Fi
devices such as the SimpleLink Wi-Fi Internet-on-a chip solution from Texas
Instruments.
SimpleLink™ CC31xx, CC32xx Wi-Fi® Internet-on-a chip™
Solution Built-In Security Features
The SimpleLink Wi-Fi CC31xx and CC32xx Internet-on-a chip
family of devices from Texas Instruments offer a wide range of built-in
security features to help developers address a variety of security needs,
which is achieved without any processing burden on the main microcontroller
(MCU). This document describes these security-related features and provides
recommendations for leveraging each in the context of practical system
implementation.
SimpleLink™ CC3135, CC3235 Wi-Fi® and
Internet-of-Things Over-the-Air Update
This document describes the OTA library for the SimpleLink
Wi-Fi CC3x35 family of devices from Texas Instruments and explains how to
prepare a new cloud-ready update to be downloaded by the OTA library.
SimpleLink™ CC3135, CC3235 Wi-Fi® Internet-on-a chip™
Solution Device Provisioning
This guide describes the provisioning process, which
provides the SimpleLink Wi-Fi device with the information (network name,
password, and so forth) needed to connect to a wireless network.
Transfer of TI's Wi-Fi® Alliance Certifications to
Products Based on SimpleLink™
This document explains how to employ the Wi-Fi® Alliance (WFA) derivative
certification transfer policy to transfer a WFA certification, already
obtained by Texas Instruments, to a system you have developed.
Using Serial Flash on SimpleLink™ CC3135 and CC3235
Wi-Fi® and Internet-of-Things Devices
This application note is divided into two parts. The first
part provides important guidelines and best- practice design techniques to
consider when choosing and embedding a serial Flash paired with the CC3135
and CC3235 (CC3x35) devices. The second part describes the file system,
along with guidelines and considerations for system designers working with
the CC3x35 devices.
More Literature
User's Guides
UniFlash SimpleLink™ CC31xx/32xx Wi-Fi® and IoC™
Solution ImageCreator and Pro
This document describes the installation, operation, and usage of the
SimpleLink ImageCreator tool as part of the UniFlash.
SimpleLink™ Wi-Fi® and Internet-of-Things CC31xx and
CC32xx Network Processor
This document provides software (SW) programmers with all
of the required knowledge for working with the networking subsystem of the
SimpleLink Wi-Fi devices. This guide provides basic guidelines for writing
robust, optimized networking host applications, and describes the
capabilities of the networking subsystem. The guide contains some example
code snapshots, to give users an idea of how to work with the host driver.
More comprehensive code examples can be found in the formal software
development kit (SDK). This guide does not provide a detailed description of
the host driver APIs.
SimpleLink™ Wi-Fi® CC3135 and CC3235 Provisioning for
Mobile Applications
This guide describes TI’s SimpleLink Wi-Fi provisioning
solution for mobile applications, specifically on the usage of the Android™ and IOS® building blocks
for UI requirements, networking, and provisioning APIs required for building
the mobile application.
CC3235 SimpleLink™ Wi-Fi® and Internet of Things
Technical Reference Manual
This technical reference manual details the modules and
peripherals of the CC3235 SimpleLink™ Wi-Fi® MCU. Each
description presents the module or peripheral in a general sense. Not all
features and functions of all modules or peripherals may be present on all
devices. Pin functions, internal signal connections, and operational
parameters differ from device to device. The user should consult the
device-specific data sheet for these details.
SimpleLink™ Wi-Fi® and Internet-on-a chip™ CC3135 and
CC3235 Solution Radio Tool
The Radio Tool serves as a control panel for direct access
to the radio, and can be used for both the radio frequency (RF) evaluation
and for certification purposes. This guide describes how to have the tool
work seamlessly on Texas Instruments evaluation platforms such as the
BoosterPack™ plus FTDI emulation board for CC3235 devices, and the
LaunchPad™ for CC3235 devices.
CC3235MOD SimpleLink™ Wi-Fi® LaunchPad™ Development
Kit
The CC3235MOD SimpleLink LaunchPad™ Development Kit
(LAUNCHCC3235MOD) is a low-cost evaluation platform for
Arm®Cortex®-M4-based MCUs. The LaunchPad design
highlights the CC3235MOD Internet-on-a chip™ solution and Dual-Band Wi-Fi
capabilities. The CC3235MOD LaunchPad also features temperature and
accelerometer sensors, programmable user buttons, an RGB LED for custom
applications, and onboard emulation for debugging. The stackable headers of
the CC3235MOD LaunchPad XL interface demonstrate how easy it is to expand
the functionality of the LaunchPad when interfacing with other peripherals
on many existing BoosterPack™ Plug-in Module add-on boards, such as
graphical displays, audio codecs, antenna selection, environmental sensing,
and more.