SCHS130D August 1997 – May 2021 CD54HC20 , CD74HC20
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Standard CMOS inputs are high impedance and are typically modeled as a resistor from the input to ground in parallel with the input capacitance given in the Section 6.5. The worst case resistance is calculated with the maximum input voltage, given in the Section 6.1, and the maximum input leakage current, given in the Section 6.5, using ohm's law (R = V ÷ I).
Signals applied to the inputs need to have fast edge rates, as defined by the input transition time in the Section 6.3 to avoid excessive current consumption and oscillations. If a slow or noisy input signal is required, a device with a Schmitt-trigger input should be used to condition the input signal prior to the standard CMOS input.