SCAS759C April 2004 – July 2017 CDCM1802
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The input of the CDCM1802 has high impedance and comes with a very large common mode voltage range. For optimized noise performance it is recommended to properly terminate the PCB trace (transmission line).
Additional termination techniques can be found in the following application notes: SCAA062 and SCAA059.
NOTE:
CAC − AC-coupling capacitor (for example, 10 nF)Figure 18 shows a fanout buffer application.
The CDCM1802 shown in Figure 18 is configured to be able to select an 100-MHz LVPECL clock from the backplane. The signal can be fanned out to desired devices, as shown. The CDCM1802 offers internal dividers for both the LVCMOS and LVPECL output. In the example the LVCMOS output is divided by 4 and the LVPECL output is divided by 1.
Refer to LVPECL Receiver Input Termination for proper input terminations, dependent on single-ended or differential inputs.
Refer to Figure 9 and Figure 10 for output termination schemes depending on the receiver application.
Refer to Table 1 for setting the desired divider modes.
Input (Vectron C5310A1) = 83 fs, rms | Output (LVPECL, divide 1) = 134 fs, rms | |||
additive jitter = 105 fs, rms (typ) |