SCAS931G May 2012 – January 2018 CDCM6208
PRODUCTION DATA.
Figure 34 shows two typical applications examples of the RESETN pin and usage of the PWR pin in Pin Mode.
Figure 34(a) SPI / I2C mode only: shows the RESETN pin connected to a digital device that controls device reset. The resistor and capacitor combination ensure reset is held low even if the CDCM6208 is powered up before the host controller output signal is valid.
Figure 34(b) SPI / I2C mode only: shows a configuration in which the user wishes to introduce a delay between the time that the system applies power to the device and the device exiting reset. If the user does not use a capacitor, then the device effectively ignores the state of the RESETN pin.
Figure 34(c) Pin mode only: shows a configuration useful if the device is used in Pin Mode. Here device pin number 44 becomes the PWR input. An external pull down resistor can be used to pull this pin down. If the resistor is not installed, the pin is internally pulled high.
Figure 35 shows how the different possible device configurations and when the VCO becomes calibrated and the outputs turn on and off.