SNAS364F May 2006 – April 2016 DAC102S085
PRODUCTION DATA.
where
Its value is 1/2 of VA.
THD is measured in dB.
This is the time from the falling edge of the 16th SCLK pulse to when the output voltage deviates from the power-down voltage of 0 V.
For related documentation, see the following:
LP2980-N Micropower 50 mA Ultra Low-Dropout Regulator In SOT-23 Package (SNOS733)
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
E2E is a trademark of Texas Instruments.
SPI is a trademark of Motorola, Inc..
All other trademarks are the property of their respective owners.
These devices have limited built-in ESD protection. The leads should be shorted together or the device placed in conductive foam during storage or handling to prevent electrostatic damage to the MOS gates.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.