SLASEQ4A October 2018 – December 2018 DAC43608 , DAC53608
PRODUCTION DATA.
The address byte, as shown in Table 2, is the first byte received following the START condition from the master device. The first four bits (MSBs) of the address are factory preset to 1001. The next 3 bits of the address are controlled by the A0 pin. The A0 pin input can be connected to VDD, AGND, SCL, or SDA. The A0 pin is sampled during the first byte of each data frame to determine the address. The device latches the value of the address pin and consequently will respond to that particular address according to Table 3.
The DACx3608 family supports broadcast addressing. Broadcast addressing can be used for synchronously updating or powering down multiple DACx3608 devices. The DACx3608 family is designed to work with other members of the family to support multichip synchronous update. Using the broadcast address, the DACx3608 devices respond regardless of the states of the address pins. Broadcast is supported only in write mode.
COMMENT | MSB | LSB | ||||||
---|---|---|---|---|---|---|---|---|
AD6 | AD5 | AD4 | AD3 | AD2 | AD1 | AD0 | R/W | |
General address | 1 | 0 | 0 | 1 | See Table 3 (slave address column) | 0 or 1 | ||
Broadcast address | 1 | 0 | 0 | 0 | 1 | 1 | 1 | 0 |
SLAVE ADDRESS | A0 PIN |
---|---|
1001 000 | AGND |
1001 001 | VDD |
1001 010 | SDA |
1001 011 | SCL |