See (1)
|
MIN |
MAX |
UNIT |
Supply voltage |
VDD |
Supply voltage
for LVCMOS core logic(2) Supply voltage for LPSDR
low-speed interface |
–0.5 |
2.3 |
V |
VDDI |
Supply voltage
for SubLVDS receivers(2) |
–0.5 |
2.3 |
VOFFSET |
Supply voltage
for HVCMOS and micromirror electrode(2)(3) |
–0.5 |
11 |
VBIAS |
Supply voltage
for micromirror electrode(2) |
–0.5 |
19 |
VRESET |
Supply voltage
for micromirror electrode(2) |
–15 |
0.5 |
|VDDI–VDD| |
Supply voltage
delta (absolute value)(4) |
|
0.3 |
|VBIAS–VOFFSET| |
Supply voltage
delta (absolute value)(5) |
|
11 |
|VBIAS–VRESET| |
Supply voltage
delta (absolute value)(6) |
|
34 |
Input voltage |
Input voltage for other inputs LPSDR(2) |
–0.5 |
VDD +
0.5 |
V |
Input voltage for other inputs SubLVDS(2)(7) |
–0.5 |
VDDI +
0.5 |
Input pins |
|VID| |
SubLVDS input
differential voltage (absolute value)(7) |
|
810 |
mV |
IID |
SubLVDS input
differential current |
|
10 |
mA |
Clock frequency |
ƒclock |
Clock
frequency for low-speed interface LS_CLK |
|
130 |
MHz |
ƒclock |
Clock
frequency for high-speed interface DCLK |
|
560 |
Environmental |
TARRAY and TWINDOW |
Temperature –
operational(8) |
–20 |
90 |
°C |
Temperature – non-operational(8) |
–40 |
90 |
TDP |
Dew point
temperature – operating and non-operating (non-condensing) |
|
81 |
|TDELTA| |
Absolute
temperature delta between any point on the window edge and the
ceramic test point TP1(9) |
|
30 |
(1) Operation outside the Absolute Maximum Ratings may cause
permanent device damage. Absolute Maximum Ratings do not imply functional
operation of the device at these or any other conditions beyond those listed
under Recommended Operating Conditions. If used outside the Recommended
Operating Conditions but within the Absolute Maximum Ratings, the device may not
be fully functional, and this may affect device reliability, functionality,
performance, and shorten the device lifetime.
(2) All voltage values are with respect to the ground terminals
(VSS). The following power supplies are all required to operate the DMD: VSS,
VDD, VDDI, VOFFSET, VBIAS, and VRESET.
(3) VOFFSET supply transients must fall within specified voltages.
(4) Exceeding the recommended allowable absolute voltage difference
between VDDI and VDD may result in excessive current draw.
(5) Exceeding the recommended allowable absolute voltage difference
between VBIAS and VOFFSET may result in excessive current draw.
(6) Exceeding the recommended allowable absolute voltage difference
between VBIAS and VRESET may result in excessive current draw.
(7) This maximum input voltage rating applies when each input of a
differential pair is at the same voltage potential. Sub-LVDS differential inputs
must not exceed the specified limit or damage may result to the internal
termination resistors.
(8) The highest temperature of the active array (as calculated by
the
Section 7.6) or of any point along the window edge as defined in
Figure 7-1. The locations of thermal test points TP2 and TP3 in
Figure 7-1 are intended to measure the highest window edge temperature. If a particular
application causes another point on the window edge to be at a higher
temperature, that point should be used.
(9) Temperature delta is the highest difference between the
ceramic test point 1 (TP1) and anywhere on the window edge as shown in
Figure 7-1. The window test points TP2 and TP3 shown in
Figure 7-1 are intended to result in the worst case delta. If a particular application
causes another point on the window edge to result in a larger delta temperature,
that point should be used.