see (1)
|
MIN |
MAX |
UNIT |
Supply voltage |
VDD |
Supply voltage for LVCMOS core logic(2)
Supply voltage for LPSDR low speed
interface |
–0.5 |
2.3 |
V |
VDDI |
Supply voltage for SubLVDS receivers(2)
|
–0.5 |
2.3 |
V |
VOFFSET |
Supply voltage for HVCMOS and micromirror
electrode(2)
(3)
|
–0.5 |
11 |
V |
VBIAS |
Supply voltage for micromirror
electrode(2) |
–0.5 |
19 |
V |
VRESET |
Supply voltage for micromirror
electrode(2)
|
–15 |
0.5 |
V |
| VDDI–VDD | |
Supply voltage delta (absolute
value)(4)
|
|
0.3 |
V |
| VBIAS–VOFFSET | |
Supply voltage delta (absolute
value)(5)
|
|
11 |
V |
| VBIAS–VRESET | |
Supply voltage delta (absolute
value)(6)
|
|
34 |
V |
Input voltage |
Input
voltage for other inputs LPSDR(2)
|
–0.5 |
VDD + 0.5 |
V |
Input
voltage for other inputs SubLVDS(2)
(7)
|
–0.5 |
VDDI + 0.5 |
V |
Input pins |
| VID | |
SubLVDS input differential voltage
(absolute value)(7)
|
|
810 |
mV |
IID |
SubLVDS input differential current |
|
10 |
mA |
Clock frequency |
ƒclock |
Clock frequency for low speed interface LS_CLK |
|
130 |
MHz |
ƒclock |
Clock frequency for high speed interface DCLK |
|
620 |
MHz |
Environmental |
TARRAY and TWINDOW |
Temperature – operational (8)
|
–20 |
90 |
°C |
Temperature –
non-operational(8)
|
–40 |
90 |
°C |
TDP |
Dew Point Temperature - operating and non-operating (non-condensing) |
|
81 |
°C |
|TDELTA| |
Absolute Temperature delta between any
point on the window edge and the ceramic test point TP1(9)
|
|
30 |
°C |
(1) Operation outside the Absolute Maximum Ratings may cause
permanent device damage. Absolute Maximum Ratings do not imply functional
operation of the device at these or any other conditions beyond those listed
under Recommended Operating Conditions. If used outside the Recommended
Operating Conditions but within the Absolute Maximum Ratings, the device may not
be fully functional, and this may affect device reliability, functionality,
performance, and shorten the device lifetime.
(2) All voltage values are with respect to the ground terminals (VSS). The following power supplies are all required to operate the DMD: VDD, VDDI, VOFFSET, VBIAS, and VRESET. All VSS connections are also required.
(3) VOFFSET supply transients must fall within specified voltages.
(4) Exceeding the recommended allowable absolute voltage difference between VDDI and VDD may result in excessive current draw.
(5) Exceeding the recommended allowable absolute voltage difference between VBIAS and VOFFSET may result in excessive current draw.
(6) Exceeding the recommended allowable absolute voltage difference between VBIAS and VRESET may result in excessive current draw.
(7) This maximum input voltage rating applies when each input of a differential pair is at the same voltage potential. Sub-LVDS differential inputs must not exceed the specified limit or damage may result to the internal
termination resistors.
(8) The highest temperature of the active array (as calculated by the
Micromirror Array Temperature Calculation) or of any point along the Window Edge as defined in
Figure 7-1. The locations of thermal test points TP2, TP3, TP4, and TP5 in
Figure 7-1 are intended to measure the highest window edge temperature. If a particular application causes another point on the window edge to be at a higher temperature, that point should be used.
(9) Temperature delta is the highest difference between the ceramic test point 1 (TP1) and anywhere on the window edge as shown in
Figure 7-1. The window test points TP2, TP3, TP4, and TP5 shown in
Figure 7-1 are intended to result in the worst case delta. If a particular application causes another point on the window edge to result in a larger delta
temperature, that point should be used.