PARAMETER |
TEST CONDITIONS |
MIN |
TYP |
MAX |
UNIT |
Micromirror tilt angle(1)(2)(3)(4)(5) |
landed state |
11 |
12 |
13 |
° |
Micromirror crossover time(6) |
typical performance |
|
2.5 |
|
us |
Micromirror switching time(7) |
typical performance |
8 |
|
|
us |
Image performance(8) |
Bright pixels(s) in active area(9) |
Gray 10 Screen(10) |
|
|
0 |
micromirrors
|
Bright pixes(s) in POM(11) |
Gray 10 Screen(10) |
|
|
1 |
micromirrors
|
Dark pixel(s) in active area(12) |
White Screen
|
|
|
4 |
micromirrors
|
Adjacent pixels(13) |
Any Screen
|
|
|
0 |
micromirrors
|
Unstable pixel(s) in active area(14) |
Any Screen
|
|
|
0 |
micromirrors
|
(1) Measured relative to the plane formed by the overall micromirror array.
(2) Represents the landed tilt angle variation relative to the nominal landed tilt angle.
(3) Represents the variation that can occur between any two individual micromirrors, located on the same device or located on different devices.
(4) For some applications, it is critical to account for the micromirror tilt angle variation in the overall system optical design. With some system optical designs, the micromirror tilt angle variation within a device may result in perceivable non-uniformities in the light field reflected from the micromirror array. With some system optical designs, the micromirror tilt angle variation between devices may result in colorimetry variations, system efficiency variations or system contrast variations.
(5) When the micromirror array is landed (not parked), the tilt direction of each individual micromirror is dictated by the binary contents of the CMOS memory cell associated with each individual micromirror. A binary value of 1 results in a micromirror landing in the ON State direction. A binary value of 0 results in a micromirror landing in the OFF State direction, see
Figure 6-16.
(6) The time required for a micromirror to nominally transition from one landed state to the opposite landed state.
(7) The minimum time between successive transitions of a micromirror.
(8) Conditions of Acceptance: All DMD image performance returns will be evaluated using the following projected image test conditions:
Test set degamma shall be linear
Test set brightness and contrast shall be set to nominal
The diagonal size of the projected image shall be a minimum of 60 inches
The projection screen shall be 1x gain
The projected image shall be inspected from an 8 foot minimum viewing distance
The image shall be in focus during all image performance tests
(9) Bright pixel definition: A single pixel or mirror that is stuck in the ON position and is visibly brighter that the surrounding pixels
(10) Gray 10 screen definition: All areas of the screen are colored with the following settings:
Red = 10/255
Green = 10/255
Blue = 10/255
(11) POM definition: Rectangular border of off-state mirror surrounding the active area.
(12) Dark pixel definition: A single pixel or mirror that is stuck in the OFF position and is visibly darker than the surrounding pixels.
(13) Adjacent pixel definition: Two or more stuck pixels sharing a common border or common point, also referred to as a cluster.
(14) Unstable pixel definition: A single pixel or mirror that does not operate in sequence with the parameters loaded into memory. The unstable pixel appears to be flickering asynchronously with the image.