DLPS240A June 2024 – August 2024 DLPA3085
PRODUCTION DATA
The DMD HV regulator generates three high-voltage supplies: DMD_VRESET, DMD_VBIAS, and DMD_VOFFSET (Figure 6-13). The DMD HV regulator uses a switching regulator (switch A-D), where the inductor is time-shared between all three supplies. The inductor is charged up to a certain current value (current limit) and then discharged into one of the three supplies. If not all supplies need charging the time available will be equally shared between those that do need charging. The recommended value for the capacitors is 1µF for VRST and VOFS, and 470nF for VBIAS. The inductor value is 10µH.