DLPS240A June 2024 – August 2024 DLPA3085
PRODUCTION DATA
The buck converter as well as the supporting LDO_BUCK have a power good indication. The buck converter has a separate indication.
The power good for the buck converter indicates if their output voltage (PWR6_FB) is within a defined window. The relative power good ratio is 72%. This means that if the output voltage is below 72% of the set voltage the PG_fault bit is set high. The power good bit of the buck converter is in Detailed Status Register1 (0x27) bit: