DLPS240A June 2024 – August 2024 DLPA3085
PRODUCTION DATA
The illumination function includes all blocks needed to generate light for the DLP system. To accurately set the current through the LEDs, a control loop is used (Figure 6-2). The intended LED current is set through IDAC[9:0]. The Illumination driver controls the LED anode voltage VLED and as a result a current will flow through one of the LEDs. The LED current is measured from the voltage across sense resistor RLIM. Based on the difference between the actual and intended current, the loop controls the output of the buck converter (VLED) higher or lower. The LED that conducts the current is controlled by switches P, Q, and R. The Openloop feedback circuitry ensures that the control loop can be closed for cases when there is no path through the LED (for instance, when ILED= 0).
Within the illumination block, the following blocks can be distinguished: