DLPS132 May 2018 DLPA4000
PRODUCTION DATA.
The DLPA4000 contains three general purpose buck converters and a supporting LDO (LDO_BUCKS). The three programmable 8-bit buck converters generate a voltage between 1 V and 5 V. The buck converters have an output current limit of 2 A. The device supports only General Purpose Buck2 (PWR6) types. Figure 16 shows one of the buck converters and the LDO_BUCKS.
The two DMD or DLPC buck converters discussed earlier in DMD Supplies have the same architecture as these three buck converters and can be configured in the same way.