DLPS132 May 2018 DLPA4000
PRODUCTION DATA.
Large switched currents flow through the wiring from the external RGB switches to the LEDs. Consider these two specifications to optimize the LED-to-RGB switches wiring layout:
Figure 32 shows the parasitic series impedances.
Currents up to 32 A can flow through the wires connecting the LEDs to the RGB switches. The layout can cause noticeable dissipation. Every 10 mΩ of series resistances implies a parasitic power dissipation of 5 W for a 32 A (avg) LED current . This dissipation can cause an increase in PCB temperature, and more importantly, deterioration of overall system efficiency.
The wiring resistance may impact the control dynamics of the LED current. The LED current control loop includes the routing resistance. The LED voltage (VLED) controlls the LED current. Use Equation 15 to calculate the total differential resistance of a path RSERIES.
where
Equation 15 ignores LSERIES because realistic values are usually sufficiently low to cause any noticeable impact on the dynamics
All differential resistance values range from about 4 mΩ to several hundreds of mΩ. Applications can yield a series resistance of 100 mΩ if the layout guidelines are not followed. Make sure the application series resistance is <10 mΩ.
The series inductance plays an important role when considering the switched nature of the LED current. the current switches through R,G and B LEDs quickly. The turn-off time is significantly fast. A current of 32 A goes to 0 A in 50 ns. This speed causes a voltage spike of approximately 1 V for every 5 nH of parasitic inductance. Minimize the series inductance of the LED wiring by designing an application that has these features:
Use a diode when the application cannot be designed to yield a sufficiently low inductance. Use a Zener diode to clamp the drain voltage of the RGB switch so that it remains below the absolute maximum rating. Choose a clamping voltage between the maximum expected VLED and the absolute maximum rating. Make sure the clamping voltage has sufficient margin relative to the minimum and maximum voltage.