DLPS048C March 2015 – June 2019 DLPC150
PRODUCTION DATA.
DLPC150 supports I2C commands through the control interface. The control interface allows another master processor to send commands to the DLPC150 chipset to query system status or perform realtime operations. The DLPC150 I2C interface ports support 100-kHz baud rate at the 7-bit address 0x1B. By definition, I2C transactions operate at the speed of the slowest device on the bus, thus there is no requirement to match the speed grade of all devices in the system.