DLPS030E December 2013 – March 2019 DLPC2607
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
The DLPC2607 device supports 100- to 120-Hz 3-D display operation, but is limited to a narrow set of configurations. 3-D operation is limited to:
To support 3-D operation, run the DLPC2607 device in Lock-to-VSYNC mode with 1× frame rate multiplication (that is, no frame rate multiplication). Each DMD frame is displayed at the source frame rate in the order it is received.
Because of the high frame rate of the source, the source line rate must be much higher than typical, but still cannot exceed the rates defined in Parallel I/F Maximum Parallel Interface Horizontal Line Rate. The minimum line rate is limited by the maximum frame rate and minimum total vertical blanking (TVB). 100- to 120-Hz Operational Limitations provides a summary of the line rate range assuming the minimum TVB.