SLLSEC6E September 2012 – June 2019 DP83848-EP
PRODUCTION DATA.
This register contains event status and enables for the interrupt function. If an event has occurred since the last read of this register, the corresponding status bit will be set. If the corresponding enable bit in the register is set, an interrupt will be generated if the event occurs. The MICR register controls must also be set to allow interrupts. The status indications in this register will be set even if the interrupt is not enabled.
BIT | BIT NAME | DEFAULT | DESCRIPTION |
---|---|---|---|
15 | RESERVED | 0, RO | RESERVED: Writes ignored, Read as 0 |
14 | ED_INT | 0, RO/COR | Energy Detect interrupt: |
1 = Energy detect interrupt is pending and is cleared by the current read | |||
0 = No energy detect interrupt pending | |||
13 | LINK_INT | 0, RO/COR | Change of Link Status interrupt: |
1 = Change of link status interrupt is pending and is cleared by the current read | |||
0 = No change of link status interrupt pending | |||
12 | SPD_INT | 0, RO/COR | Change of speed status interrupt: |
1 = Speed status change interrupt is pending and is cleared by the current read | |||
0 = No speed status change interrupt pending | |||
11 | DUP_INT | 0, RO/COR | Change of duplex status interrupt: |
1 = Duplex status change interrupt is pending and is cleared by the current read | |||
0 = No duplex status change interrupt pending | |||
10 | ANC_INT | 0, RO/COR | Auto-Negotiation Complete interrupt: |
1 = Auto-negotiation complete interrupt is pending and is cleared by the current read | |||
0 = No Auto-negotiation complete interrupt pending | |||
9 | FHF_INT | 0, RO/COR | False Carrier Counter half-full interrupt: |
1 = False carrier counter half-full interrupt is pending and is cleared by the current read | |||
0 = No false carrier counter half-full interrupt pending | |||
8 | RHF_INT | 0, RO/COR | Receive Error Counter half-full interrupt: |
1 = Receive error counter half-full interrupt is pending and is cleared by the current read | |||
0 = No receive error carrier counter half-full interrupt pending | |||
7 | RESERVED | 0, RO | RESERVED: Writes ignored, Read as 0 |
6 | ED_INT_EN | 0, RW | Enable Interrupt on energy detect event |
5 | LINK_INT_EN | 0, RW | Enable Interrupt on change of link status |
4 | SPD_INT_EN | 0, RW | Enable Interrupt on change of speed status |
3 | DUP_INT_EN | 0, RW | Enable Interrupt on change of duplex status |
2 | ANC_INT_EN | 0, RW | Enable Interrupt on Auto-negotiation complete event |
1 | FHF_INT_EN | 0, RW | Enable Interrupt on False Carrier Counter Register half-full event |
0 | RHF_INT_EN | 0, RW | Enable Interrupt on Receive Error Counter Register half-full event |