SNLS484H February 2015 – June 2024 DP83867CR , DP83867IR
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
BIT | BIT NAME | DEFAULT | DESCRIPTION |
---|---|---|---|
15:11 | RESERVED | 0, RO | RESERVED |
10:8 | RESERVED | 0x2, RW | RESERVED |
7 | RESERVED | 0, RO | RESERVED |
6:4 | RESERVED | 0x2, RW | RESERVED |
3 | RESERVED | 0, RO | RESERVED |
2:0 | ENERGY_LOST_FLD_THR | 0x1, RW | Energy Lost Threshold for FLD Energy Lost Mode ENERGY_LOST_FLD_THR will be asserted if energy detector accumulator falls below this threshold. When using strap to enable FLD feature, this bit defaults to 0x2. Register write is needed to change it to 0x1. Changing the field to other value is not advised. |