SLVSF30A October 2019 – October 2021 DRV10982-Q1
PRODUCTION DATA
If the motor suddenly becomes locked, motor speed and Ktc are not able to be refreshed because the BEMF zero cross of the motor may not appear after the lock. In this condition, lock can also be detected by the following scheme: if the current commutation period is 2× longer than the previous period.