SLVSF30A October 2019 – October 2021 DRV10982-Q1
PRODUCTION DATA
If the motor is stationary, the commutation logic must be initialized to be in phase with the position of the motor. The DRV10982-Q1 device provides for two options to initialize the commutation logic to the motor position. Initial position detect (IPD) determines the position of the motor based on the deterministic inductance variation, which is often present in BLDC motors. The align-and-go technique forces the motor into alignment by applying a voltage across a particular motor phase to force the motor to rotate in alignment with this phase.