SLOS866F May 2014 – March 2018 DRV2604L
PRODUCTION DATA.
If the impedance at the output pin of the DRV2604L device is too low, the device latches the over-current flag (OC_DETECT bit in register 0x00) and shuts down. The device periodically monitors the status of the short and remains in this condition until the short is removed. When the short is removed, the DRV2604L device restarts in the default state.