SLIS150M March 2014 – June 2024 DRV5013
PRODUCTION DATA
If the device is powered on with a magnetic flux density between BRP and BOP, then the device output is indeterminate and can either be Hi-Z or Low. If the magnetic flux density is greater than BOP, then the output is pulled low (released high for the inverted ND version). If the magnetic flux density is less than BRP, then the output is released high according to the output reference voltage and pullup resistor (pulled low for the inverted ND version).