SLASEV7 August 2020 – MONTH DRV5825P
PRODUCTION DATA
The PCB footprint (also known as a symbol or land pattern) communicates to the PCB fabrication vendor the shape and position of the copper patterns to which the DRV5825P device is soldered. This footprint can be followed directly from the guidance in the package addendum at the end of this data sheet. It is important to make sure that the thermal pad, which connects electrically and thermally to the PowerPAD™ of the DRV5825P device, be made no smaller than what is specified in the package addendum. This ensures that the DRV5825P device has the largest interface possible to move heat from the device to the board.
The via pattern shown in the package addendum provides an improved interface to carry the heat from the device through to the layers of the PCB, because small diameter plated vias (with minimally-sized annular rings) present a low thermal-impedance path from the device into the PCB. Once into the PCB, the heat travels away from the device and into the surrounding structures and air. By increasing the number of vias, as shown in the Section 11.2 section, this interface can benefit from improved thermal performance.
Vias can obstruct heat flow if they are not constructed properly.
More notes on the construction and placement of vias are as follows: