SLVSE38A April 2018 – July 2018 DRV8306
PRODUCTION DATA.
The GHx and GLx pins are monitored such that if the voltage on the external MOSFET gate does not increase or decrease after the tDRIVE time, a gate driver fault is detected. This fault may be encountered if the GHx or GLx pins are shorted to the PGND, SHx, or VM pins. Additionally, a gate driver fault may be encountered if the selected IDRIVE setting is not sufficient to turn on the external MOSFET within the tDRIVE period. After a gate drive fault is detected, all external MOSFETs are disabled and the nFAULT pin is driven low. Normal operation resumes (gate driver operation and the nFAULT pin is released) when the gate driver fault condition is removed.
Gate driver faults can indicate that the selected IDRIVE or tDRIVE settings are too low to slew the external MOSFET in the desired time. Increasing either the IDRIVE or tDRIVE setting can resolve gate driver faults in these cases. Alternatively, if a gate-to-source short occurs on the external MOSFET, a gate driver fault is reported because of the MOSFET gate not turning on.