SLVSE38A April 2018 – July 2018 DRV8306
PRODUCTION DATA.
The current-limit circuit activates if the voltage detected across the low-side sense resistor (ISEN pin) exceeds the VLIMIT voltage. This feature restricts motor current to less than the VLIMIT voltage divided by the RSENSE resistance.
NOTE
The current-limit circuit is ignored immediately after the PWM signal goes active for a short blanking time to prevent false trips of the current-limit circuit.
If the current limit activates, the high-side FET is disabled until the beginning of the next PWM cycle. Because the synchronous rectification is always enabled, when the current limit activates, the low-side FET is activated while the high-side FET is disabled.