SLVSGI0B september 2022 – july 2023 DRV8411
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The trip current (ITRIP) is the maximum current driven through either winding. Because the peak current (start current) of the motor is 900 mA, the ITRIP current level is selected to be just greater than the peak current. The selected ITRIP value for this example is 1 A. Therefore, use Equation 4 to select the value of the sense resistors (RSENSE_A and RSENSE_B) connected to the AISEN and BISEN pins.