SLVSHA4 June 2024 DRV8421
PRODUCTION DATA
An analog current limit circuit on each FET limits the current through the FET by limiting the gate drive. If this analog current limit persists for longer than the OCP deglitch time tOCP, all FETs in the H-bridge are disabled. In addition, in DRV8421B, the nFAULT pin is driven low. The device remains disabled until the retry time tRETRY occurs. The OCP is independent for each H-bridge.
Overcurrent conditions are detected independently on both high-side and low-side devices; that is, a short to ground, supply, or across the motor winding all result in an OCP event.