SLOSE55C May 2020 – July 2022 DRV8426
PRODUCTION DATA
During PWM current chopping, the H-bridge is enabled to drive through the motor winding until the PWM current chopping threshold is reached. This is shown in Figure 7-7, Item 1.
Once the chopping current threshold is reached, the H-bridge can operate in two different states, fast decay or slow decay. In fast decay mode, once the PWM chopping current level has been reached, the opposite FETs are turned on and the H-bridge reverses state to allow winding current to flow in a reverse direction. Fast decay mode is shown in Figure 7-7, item 2. In slow decay mode, winding current is re-circulated by enabling both of the low-side FETs in the bridge. This is shown in Figure 7-7, Item 3.
The decay mode of the DRV8426 is selected by the DECAY0 and DECAY1 pins as shown in Table 7-6. If DECAY1 pin is Hi-Z, irrespective of the DECAY0 pin voltage, the decay mode will be smart tune dynamic decay. The decay modes can be changed on the fly. After a decay mode change, the new decay mode is applied after a 10 µs de-glitch time.
DECAY0 | DECAY1 | INCREASING STEPS | DECREASING STEPS |
---|---|---|---|
0 | 0 | Smart tune Dynamic Decay | Smart tune Dynamic Decay |
0 | 1 | Smart tune Ripple Control | Smart tune Ripple Control |
1 | 0 | Mixed decay: 30% fast | Mixed decay: 30% fast |
1 | 1 | Slow decay | Mixed decay: 30% fast |
Hi-Z | 0 | Mixed decay: 60% fast | Mixed decay: 60% fast |
Hi-Z | 1 | Slow decay | Slow decay |
Figure 7-8 defines increasing and decreasing current. For the slow-mixed decay mode, the decay mode is set as slow during increasing current steps and mixed decay during decreasing current steps. In full step and noncircular 1/2-step operation, the decay mode corresponding to decreasing steps is always used.