SLOSE56B May 2020 – May 2022 DRV8426E
PRODUCTION DATA
The current through the motor windings is regulated by an adjustable, off-time PWM current-regulation circuit. When an H-bridge is enabled, current rises through the winding at a rate dependent on the DC voltage, inductance of the winding, and the magnitude of the back EMF present. When the current hits the current regulation threshold, the bridge enters a decay mode for a period of time determined by the TOFF pin setting to decrease the current. After the off-time expires, the bridge is re-enabled, starting another PWM cycle.
TOFF | OFF-TIME tOFF |
---|---|
0 | 7 µs |
1 | 16 µs |
Hi-Z | 24 µs |
330kΩ to GND | 32 µs |
The TOFF pin configures the PWM OFF time for all decay modes except smart tune ripple control. The OFF time settings can be changed on the fly. After a OFF time setting change, the new OFF time is applied after a 10 µs de-glitch time.
The current regulation threshold is set by a comparator which monitors the voltage across the current sense MOSFETs in parallel with the low-side power MOSFETs. To generate the reference voltage for the comparator, the VREFx input is attenuated by a factor of Kv.
The current regulation threshold (IREG) can be calculated as IREG (A) = VREFx (V) / KV (V/A) = VREFx (V) / 2.2 (V/A).