SLOSE48 December 2020 DRV8434A
PRODUCTION DATA
The DRV8434A operates with smart tune ripple control decay mode, which uses only slow decay during PWM current regulation. The PWM regulation current is set by a comparator which monitors the voltage across the current sense MOSFETs in parallel with the low-side power MOSFETs. The current sense MOSFETs are biased with a reference current that is the output of a current-mode sine-weighted DAC whose full-scale reference current is set by the voltage at the VREF pin.
The full-scale regulation current (IFS) can be calculated as IFS (A) = VREF (V) / KV (V/A) = VREF (V) / 1.32 (V/A).
During PWM current chopping, the H-bridge is enabled to drive a current through the motor winding until the PWM current chopping threshold is reached. Thereafter, the winding current is re-circulated by enabling both low-side MOSFETs of the H-bridge.